cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1 and SLEEPONEXIT

MikeAtETI
Associate III
Posted on March 18, 2013 at 16:29

Has anyone used SLEEPONEXIT around the STM32L1* family to enable it to put the micro to a STOP level and only wake up when there is a timed-based interrupt to happen?

#stm32l1-rtc-sleeponexit
1 REPLY 1
Posted on March 18, 2013 at 17:29

It's documented to exit STOP via an EXTI source, no clocks or timers are running. An alarm on the RTC running via LSE perhaps?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..