cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L0Cube UART HAL pulls in extraneous floating point code

tony2399
Associate II
Posted on October 30, 2016 at 18:47

Hi,

The latest STM32L0Cube UART Hal pulls in unnecessary floating point code when initializing the UART. The culprit is the __DIV_LPUART macro, which contains a floating point number (256.0). When replaced with the version from STM32L4Cube, it no longer pulls in floating point libraries.

The extra code takes up at least 6KB of extra code space, which is a lot for the smaller L0's.

Tony

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Anders Dam Kofoed
Associate III
Posted on December 14, 2016 at 22:18

https://community.st.com/0D70X000006SJVESA4