STM32L Vector Table definition problem in stm32l1xx.h
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-07-25 12:25 AM
Posted on July 25, 2013 at 09:25
Hello all,
I am using the stm32l1xx.h file V1.1.1 released on 09-March-2012.In the header file, STM32L specific Interrupt Numbers for medium+ density devices are defined as follows,#ifdef STM32L1XX_MDP TIM7_IRQn = 44, /*!< TIM7 global Interrupt */ TIM5_IRQn = 46, /*!< TIM5 global Interrupt */ SPI3_IRQn = 47, /*!< SPI3 global Interrupt */ DMA2_Channel1_IRQn = 50, /*!< DMA2 Channel 1 global Interrupt */ DMA2_Channel2_IRQn = 51, /*!< DMA2 Channel 2 global Interrupt*/ DMA2_Channel3_IRQn = 52, /*!< DMA2 Channel 3 global Interrupt*/ DMA2_Channel4_IRQn = 53, /*!< DMA2 Channel 4 global Interrupt*/ DMA2_Channel5_IRQn = 54, /*!< DMA2 Channel 5 global Interrupt */ AES_IRQn = 55, /*!< AES global Interrupt */ COMP_ACQ_IRQn = 56 /*!< Comparator Channel Acquisition global Interrupt*/#endifBut according to data sheet DocID15965 Rev 8, Table 36 on Page 193 interrupt channels are positioned as below.44 - TIM7 global interrupt 45 - TIM5 Global interrupt 46 - SPI3 Global interrupt 47 - DMA2 Channel 1 interrupt 48 - DMA2 Channel 2 interrupt 49 - DMA2 Channel 3 interrupt50 - DMA2 Channel 4 interrupt 51 - DMA2 Channel 5 interrupt 52 - AES global interrupt 53 - Comparator Channel Acquisition Interrupt So there is some mismatching in the provided stm32l1xx.h header file. Has anybody come across this point earlier?Regards,Anuradha
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0