2026-04-21 6:54 AM - last edited on 2026-04-21 7:12 AM by Peter BENSCH
Hello Peter ,
Need your expert reply
As we see , the confusion on N AND no N HAS MADE many of us wonder , if these can be used as interchangeable parts . Since Data Sheet does not explain , much on them ,But a search explains a compact Solution in Io's for a design flexibility .
As both have same Packages and Pin Count .
We are in need for DESIGN - STM32G0B1CBT3N , but seems to be difficult to procure . Is this Manufactured or is it rare . We only See STM32G0B1CBT6N
Regards
Nitin
2026-04-21 7:25 AM
Welcome @Tintin33, to the community!
By looking at the product website for the STM32G0B1CB, it can be seen that there is currently no STM32G0B1CBT3N (-40...+125°C). At present, therefore, you only have the option of using the STM32G0B1CBT6N (-40...+85°C).
If you absolutely need the wider temperature range, you will need to clarify availability with your local distributor, which will in any case require a minimum order quantity to release this variant - assuming that this is even possible at high temperatures because of the added functionality (VDDIO2 and UCPD).
Hope that helps?
Regards
/Peter