cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f769 maximum dsi resolution

echelon2010
Associate II
Posted on March 25, 2016 at 14:39

Hello! I want to connect tft display with 1280*720 resolution via DSI interface. TFT panel has 4 differential inputs for data. There is no reference manual for stm32f769 controller on this page http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1858/LN1999, so i don't know, what is the maximum resolution for DSI interface. Can i use such lcd with stm32f769 controller? Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nesrine M_O
Lead II
Posted on March 25, 2016 at 15:07

Hi dmitriev.artyomNo,

As it is mentioned in the STM32F769xx related data brief the MIPI® DSI host controller supports up to 720p 30 Hz resolution.

If you need more information please contact your FAE or local representative.

-Syrine-

echelon2010
Associate II
Posted on March 29, 2016 at 08:24

So it is not possible to control lcds with more than 2 data lines? Is it right?