cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f429 sdio bootloader

er3481
Senior
Posted on May 13, 2016 at 15:42

Hi,

I want to update firmware by using the sd card with my stm32f429 mcu. I will connect the sd card to mcu sdio pins ( 1 bit only) , so i will not use spi port for sd card. I just want to learn whether it is possible to update firmware by using sdio connection (not with spi) or not. (In application note the bootloader operation can be used by using the communication port peripherals ( USART, I2C, SPI, CANBUS, USB) )

http://www2.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

#been-there-done-that
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 13, 2016 at 16:12

No, the system loader in ROM does not support SDIO or SDCard update methods. You'd have to implement your own, it can be done in under 16K using the first sector/block of flash.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..