cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407 + expansion board ethernet

nikola1010
Associate II
Posted on November 22, 2015 at 14:49

Hi all,

I am trying to create stm32CubeMX project to use with stm32f407 with expansion board ethernet but except lights going on ethernet port nothing happens when trying to use socket API with FreeRTOS.

Also tried without FreeRTOS but no go.

Could someone please build CubeMX project and share it.

Big thanks in advance.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on November 22, 2015 at 16:23

Some random board, or a specific one like the

http://www.st.com/web/catalog/tools/FM146/CL1984/SC720/SS1462/PF255417?sc=stm32f4dis-expansion

? Be specific, and provide a cite.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nikola1010
Associate II
Posted on November 22, 2015 at 20:53

EDIT: sorry for bad post, tried to do it from phone - big fail!

First tnx for quick replay.

To answer your question, yes I am using that specific board.

I am trying to make CubeMX provide default template for ethernet (with and without FreeRTOS) and then:

1) ping device (wasn't successful)

2) telnet to port (eg. 8080) and get answer from uC ''yes it works'' (also unsuccessful)