cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 SPI3 interrupt problem

dancan_emre
Associate
Posted on July 08, 2014 at 08:25

Hello;

I am working on stm discovery. My aim is get output from speaker. I did it in main function. but i want to use SPI3 interrupt for send data. My codes in below. The code does not go to interrupt. I put breakpoint but its not work. I couldnt find my fault. Could anybody help me?

Thanks for your answers. 

This is my codec init, its work fine when i send data to codec in main.

void codec_init()

{

GPIO_InitTypeDef PinInitStruct;

GPIO_StructInit(&PinInitStruct);

PinInitStruct.GPIO_Pin = CODEC_RESET_PIN;

PinInitStruct.GPIO_Mode = GPIO_Mode_OUT;

PinInitStruct.GPIO_PuPd = GPIO_PuPd_DOWN;

PinInitStruct.GPIO_OType = GPIO_OType_PP;

PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOB, ENABLE);

GPIO_Init(GPIOD, &PinInitStruct);

PinInitStruct.GPIO_Mode = GPIO_Mode_AF;

PinInitStruct.GPIO_OType = GPIO_OType_OD;

PinInitStruct.GPIO_Pin = I2C_SCL_PIN | I2C_SDA_PIN;

PinInitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOB, &PinInitStruct);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_I2C1);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1 | RCC_APB1Periph_SPI3, ENABLE);

RCC_PLLI2SCmd(ENABLE);

PinInitStruct.GPIO_OType = GPIO_OType_PP;

PinInitStruct.GPIO_Pin = I2S3_SCLK_PIN | I2S3_SD_PIN | I2S3_MCLK_PIN;

GPIO_Init(GPIOC, &PinInitStruct);

PinInitStruct.GPIO_Pin = I2S3_WS_PIN;

GPIO_Init(GPIOA, &PinInitStruct);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI3);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_SPI3);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3);

GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SPI3);

//keep Codec off for now

GPIO_ResetBits(GPIOD, CODEC_RESET_PIN);

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_3);

NVIC_InitStructure2.NVIC_IRQChannel = SPI3_IRQn;

NVIC_InitStructure2.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure2.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure2.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure2);

// configure I2S port

SPI_I2S_DeInit(CODEC_I2S);

I2S_InitType.I2S_AudioFreq = I2S_AudioFreq_16k;

I2S_InitType.I2S_MCLKOutput = I2S_MCLKOutput_Enable;

I2S_InitType.I2S_DataFormat = I2S_DataFormat_16b;

I2S_InitType.I2S_Mode = I2S_Mode_MasterTx;

I2S_InitType.I2S_Standard = I2S_Standard_Phillips;

I2S_InitType.I2S_CPOL = I2S_CPOL_Low;

I2S_Init(CODEC_I2S, &I2S_InitType);

        I2S_FullDuplexConfig(I2S3ext, &I2S_InitType);

  

// configure I2C port

I2C_DeInit(CODEC_I2C);

I2C_InitType.I2C_ClockSpeed = 100000;

I2C_InitType.I2C_Mode = I2C_Mode_I2C;

I2C_InitType.I2C_OwnAddress1 = CORE_I2C_ADDRESS;

I2C_InitType.I2C_Ack = I2C_Ack_Enable;

I2C_InitType.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

I2C_InitType.I2C_DutyCycle = I2C_DutyCycle_2;

I2C_Cmd(CODEC_I2C, ENABLE);

I2C_Init(CODEC_I2C, &I2C_InitType);

  SPI_I2S_ITConfig(SPI3, SPI_I2S_IT_TXE, ENABLE);

}

void I2S3_IRQHANDLER(void) {

if(SPI_GetITStatus(SPI3, SPI_I2S_IT_TXE) != RESET)

{SPI_I2S_SendData(SPI3,Buffer[counter]);} 

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 09, 2014 at 22:11

void I2S3_IRQHANDLER(void) {

Case sensitive, use SPI3_IRQHandler ? Or perhaps you have some #define you haven't shared?

If you use C++ make sure it's not mangling the name, review .MAP file
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..