cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f4 rs232 IAR IDE

achourwissem
Associate II
Posted on June 02, 2013 at 13:34

hello :)

i had a problem  when i send a character or receive a character , i always get a wrong character like ''-'' or a heart ...

ps: i'm using rs232 -> USB converter

here is my code:

&sharpinclude ''stm32f4xx.h''

void main()

{

 //UART4 initialization

RCC->APB1ENR |= 0x00080000; // Enable clock for UART4

RCC->AHB1ENR |= 0x00000004; // Enable clock for GPIOC

GPIOC->MODER |= 0x00a00000; // PC10, PC11 => AF mode

GPIOC->AFR[1] |= 0x00008800; // select AF8 (UART4,5,6) for PA10, PA11

UART4->BRR = 0x1120; // 9600 baud

UART4->CR1 |= 0x200c; // Enable UART for TX, RX

UART4->CR1 |= 0x0020; // Enable RX interrupt

while(1){

  if (UART4->SR & 0x0080) {

   UART4->DR='a';

   for (int i=0; i<10000000; i++) {};

  }

}

}

please any help! :(

#too-vague
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on June 02, 2013 at 16:23

please any help!

With register level code you really own your own problems. The baud rate value looks wrong, For a chip running at 168 MHz, and APB1 at 42 MHz, 0x1117 would be better for actually getting 9600 baud. Why would you enable a receive interrupt?

// STM32 UART4 (Tx PC.10, Rx PC.11) STM32F4 Discovery - sourcer32@gmail.com
// PC11 technically conflicts with SCLK on CS43L22
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* UART4 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
}
/**************************************************************************************/
void UART4_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART4, &USART_InitStructure);
USART_Cmd(UART4, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
UART4_Configuration();
while(1)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(UART4, 0x49); // Send 'I'
}
while(1); // Don't want to exit
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
achourwissem
Associate II
Posted on June 02, 2013 at 21:17

thnx for your reply! :)

but it still didnt work for me :\ even i changed the baud rate to many values

Posted on June 03, 2013 at 04:41

In that case you'll need to pay particular attention to the crystal on the board, the define for HSE_VALUE, and the PLL settings in system_stm32f4xx.c. Most notably, the STM32F4-Discovery board uses an 8 MHz crystal, and most of ST's other offerings use a 25 MHz crystal. Failing to deal with this will result in baud rates being wrong, I highly recommend sending characters repetitively and measuring the bit time with a scope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
achourwissem
Associate II
Posted on June 03, 2013 at 23:30

thnx clive for urr answer :) this is my config in system_stm32f4xx.c and plz tell me what can i do

 This file configures the system clock as follows:

  *=============================================================================

  *=============================================================================

  *        Supported STM32F4xx device revision    | Rev A

  *-----------------------------------------------------------------------------

  *        System Clock source                    | PLL (HSE)

  *-----------------------------------------------------------------------------

  *        SYSCLK(Hz)                             | 168000000

  *-----------------------------------------------------------------------------

  *        HCLK(Hz)                               | 168000000

  *-----------------------------------------------------------------------------

  *        AHB Prescaler                          | 1

  *-----------------------------------------------------------------------------

  *        APB1 Prescaler                         | 4

  *-----------------------------------------------------------------------------

  *        APB2 Prescaler                         | 2

  *-----------------------------------------------------------------------------

  *        HSE Frequency(Hz)                      | 25000000

  *-----------------------------------------------------------------------------

  *        PLL_M                                  | 25

  *-----------------------------------------------------------------------------

  *        PLL_N                                  | 336

  *-----------------------------------------------------------------------------

  *        PLL_P                                  | 2

  *-----------------------------------------------------------------------------

  *        PLL_Q                                  | 7

  *-----------------------------------------------------------------------------

  *        PLLI2S_N                               | NA

  *-----------------------------------------------------------------------------

  *        PLLI2S_R                               | NA

  *-----------------------------------------------------------------------------

  *        I2S input clock                        | NA

  *-----------------------------------------------------------------------------

  *        VDD(V)                                 | 3.3

  *-----------------------------------------------------------------------------

  *        Main regulator output voltage          | Scale1 mode

  *-----------------------------------------------------------------------------

  *        Flash Latency(WS)                      | 5

  *-----------------------------------------------------------------------------

  *        Prefetch Buffer                        | OFF

  *-----------------------------------------------------------------------------

  *        Instruction cache                      | ON

  *-----------------------------------------------------------------------------

  *        Data cache                             | ON

  *-----------------------------------------------------------------------------

  *        Require 48MHz for USB OTG FS,          | Enabled

  *        SDIO and RNG clock                     |

  *-----------------------------------------------------------------------------
Posted on June 04, 2013 at 00:07

Do you have an STM32F4-Discovery board? I've kind of assumed this, but you've not explicitly stated what you're using.

If so you'll need to modify the PLL_M define to 8 in this file, and define HSE_VALUE as 8000000 within the project.

In Keil it would be Options -> C/C++ -> Preprocessor Symbols -> Define

Should be something like : STM32F4XX, USE_STDPERIPH_DRIVER, HSE_VALUE=8000000

For IAR you'll need to read your manuals.

Make sure it's not redefined in any other source files.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
achourwissem
Associate II
Posted on June 04, 2013 at 13:08

thnx! i think i'm near to the good results , because it changed a little and the characters are better but still wrong , i changed the PLL_M to 8 and HSE to 8Mhz , i think it still something missing :)

should i change also the APB1 Prescaler or no ? and what is the new baud rate value i should put it ? 
achourwissem
Associate II
Posted on June 04, 2013 at 13:09

and yeah i'm using STM32F4

Posted on June 04, 2013 at 13:34

Have you checked the bit timing with a scope?

Why would you need to change the APB settings? The PLL value being changed is the one that generates the 1 MHz comparison frequency internally. The other setting should get us to 168 MHz. The startup_stm32f4xx.s code calls the SystemInit() routine in system_stm32f4xx.c, and it is this code that should set up the pll and buses.

You could also use timers, and MCO pins to confirm internal clock speeds with a scope.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
achourwissem
Associate II
Posted on June 04, 2013 at 20:29

anyway i dont have scope to test on it , i'm little confused what to do

thnx anyway clive :)