STM32F4 HAL USART Interrupt over run error
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-03-02 4:00 AM
Posted on March 02, 2015 at 13:00
I am trying to receive GPS data over USART. I previously attempted ''polling mode'' which produced garbled/corrupted output. Now trying interrupt mode without success. I am also using FreeRTOS.
```#define RXBUFFERSIZE 1
uint8_t aRxBuffer[RXBUFFERSIZE];int task() { status = HAL_UART_Receive_IT(&huart1, (uint8_t *) aRxBuffer, RXBUFFERSIZE); if (status != 0) __BKPT(0);}extern ''C'' {void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { HAL_StatusTypeDef status; uint8_t data; osMessagePut(usartQueue, aRxBuffer[0], 0); status = HAL_UART_Receive_IT(&huart1, (uint8_t *) aRxBuffer, RXBUFFERSIZE); if (status != 0) __BKPT(0);}}```When `HAL_UART_IRQHandler(UART_HandleTypeDef *huart)` is called from the interrupt callback, the the over run error occurs which is the result of this code:```
tmp1 = __HAL_UART_GET_FLAG(huart, UART_FLAG_ORE); tmp2 = __HAL_UART_GET_IT_SOURCE(huart, UART_IT_ERR); /* UART Over-Run interrupt occurred ----------------------------------------*/ if((tmp1 != RESET) && (tmp2 != RESET)) { __HAL_UART_CLEAR_OREFLAG(huart); huart->ErrorCode |= HAL_UART_ERROR_ORE; }```What could be the cause?Thank you :)
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0