2014-08-22 10:27 PM
Hi.
I have tried to build a project using the provided source code in Eclipse IDE. I could do simple live recording and play back from Internal Flash. But I got the following errors when using USB for recording and playback(ST provided demo) . ../src/USB/usb_dcd.c:93:7: error: 'USB_OTG_CORE_HANDLE' has no member named 'dev' pdev->dev.device_status = USB_OTG_DEFAULT; Can any one help me to fix these errors.2014-08-23 3:41 AM
Why are you even using this file? The ST example doesn't.
Look, if you insist on using tool chains which are not supported directly, you're going to have to get a lot keener about looking at how other support tools projects are built, by examining project and make files, and perhaps even downloading eval versions of other tool chains if you can't figure out how to read ASCII/XML project descriptions.