cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Discovery CAN pin config

mrazek
Associate II
Posted on December 04, 2012 at 18:48

Dear all,

I am looking forward solution of my problem. I have successfully configured CAN driver in loopback mode, but when I want to connect to physical layer (MCP2551 I/C), there is no output on pins.

#define CANx                       CAN1

#define CAN_FILTER_NMR           0

#define CAN_CLK                    RCC_APB1Periph_CAN1

#define CAN_RX_PIN                 GPIO_Pin_0

#define CAN_TX_PIN                 GPIO_Pin_1

#define CAN_GPIO_PORT              GPIOB

#define CAN_GPIO_CLK               RCC_AHB1Periph_GPIOD

#define CAN_AF_PORT                GPIO_AF_CAN1

#define CAN_RX_SOURCE              GPIO_PinSource0

#define CAN_TX_SOURCE              GPIO_PinSource1

/* Enable the CAN controller interface clock  */

RCC_AHB1PeriphClockCmd(CAN_GPIO_CLK, ENABLE);

RCC_APB1PeriphClockCmd(CAN_CLK, ENABLE);

/* CAN pins configuration */

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.GPIO_Pin = CAN_RX_PIN | CAN_TX_PIN;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // Push - pull

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_Init(CAN_GPIO_PORT, &GPIO_InitStructure);

GPIO_PinAFConfig(CAN_GPIO_PORT, CAN_TX_SOURCE, CAN_AF_PORT);

GPIO_PinAFConfig(CAN_GPIO_PORT, CAN_RX_SOURCE, CAN_AF_PORT);

        /* Initialisation of CAN */

CAN_DeInit(CANx);

CAN_InitTypeDef CAN_InitStructure;

CAN_StructInit(&CAN_InitStructure);

CAN_InitStructure.CAN_TTCM = DISABLE;

CAN_InitStructure.CAN_ABOM = ENABLE; // Automatic bus off managment

CAN_InitStructure.CAN_AWUM = DISABLE;

CAN_InitStructure.CAN_NART = DISABLE;

CAN_InitStructure.CAN_RFLM = DISABLE;

CAN_InitStructure.CAN_TXFP = ENABLE;

CAN_InitStructure.CAN_Prescaler = 10; // 500 kbps for 42 MHz,

CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;

CAN_InitStructure.CAN_BS1 = CAN_BS1_6tq;

CAN_InitStructure.CAN_BS2 = CAN_BS2_1tq;

#ifdef CAN_LOOPBACK

CAN_InitStructure.CAN_Mode = CAN_Mode_LoopBack;

#else

CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;

#endif

uint8_t status = CAN_Init(CANx, &CAN_InitStructure);

I don't know, where the problem may be. I have tested output with oscilloscope and there is no change on the wires.

And the second question - can I connect RX and TX pin to simulate LoopBack mode? (LoopBack mode works fine, but I want to check output). I'm using USB CDC driver, but I have already disabled it and there is no change.

This is my first experience with CAN bus, but  I'm desperate from it for 2 weeks.
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on December 04, 2012 at 19:01

So is it B or D?

#define CAN_GPIO_PORT              GPIOB

#define CAN_GPIO_CLK               RCC_AHB1Periph_GPIOD

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mrazek
Associate II
Posted on December 04, 2012 at 19:27

This is only copy-paste error. In code I have D in both cases. I tested CAN1 and CAN2 too, but without any progress.

mrazek
Associate II
Posted on December 04, 2012 at 20:34

The problem is in transmitting. After 3 packets it causes an NoMailbox error.

mrazek
Associate II
Posted on December 07, 2012 at 08:15

So I have found solution of the problem. The problem was in timing. I have go throw these points:

1) I have checked CAN1 error code register (there was ACK problem)

2) I have switch CAN to loopback mode and check output on Tx PIN and on the CAN bus (there was rectangle signal)

3) I have with brute force find settings to communicate with the device

#ifdef NO_USB

pres=12;

sjw=0;

bs1=7;

bs2=4;

STM_EVAL_LEDInit(LED6);

CAN_SetParameters(pres, sjw, bs1, bs2);

CAN_SetFilter();

#endif

while (1)

{

#ifdef NO_USB

Delay(100);

CanTxMsg msg;

msg.StdId = 0x080;

msg.ExtId = 0;

msg.IDE = CAN_ID_STD;

msg.RTR = CAN_RTR_DATA;

msg.DLC = 0x04;

msg.Data[0] = 0x00;

msg.Data[1] = 0x00;

msg.Data[2] = 0x07;

msg.Data[3] = 0x00;

if (CAN_Transmit(CANx, &msg) == CAN_TxStatus_NoMailBox)

{

if(++bs2>0x07)

{

bs2=1;

if(++bs1>0x0F)

{

bs1=1;

if(++sjw>0x03)

{

sjw=1;

if(++pres>60)

{

pres++;

}

}

}

}

STM_EVAL_LEDToggle(LED6);

CAN_CancelTransmit(CANx, 0);

CAN_CancelTransmit(CANx, 1);

CAN_CancelTransmit(CANx, 2);

CAN_SetParameters(pres, sjw, bs1, bs2);

CAN_SetFilter();

}

#endif

}

4) I have made table to solve counting comm parameters (the problem was in setting APB1 clk divider to 2, so the frequency of CAN wasn't 42 but 84 MHz. The table is attached to this post.

rm239955
Associate II
Posted on November 24, 2014 at 17:10

Hallo

          Can you please tell me how did you solve the timing problem of STM32F429.I am using TJA1041A CAN transreceiver and even I am facing Acknowledgment error problem.

Can you please help me out

Thanks 

Posted on November 24, 2014 at 20:29

I wouldn't rely on someone with 4 posts 2 years ago who had to brute force setting because the math was too hard, as an effective source for a solution where the parameters are not identical. Understand how the hardware, and its clocks are derived, and you'll be in a lot stronger position.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Stm32f407%20Can%20bus%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx&currentviews=48]cross-post
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..