2015-04-18 3:44 AM
Hi,
I am trying to run the Audio playback and recording example from the firmware and drivers download package for the STM32F4 discovery. I want to use the audio file stored in the mcus internal flash, and have uncommented what I thought was the neccesary line in main.h as follows: /* Select the media where the Wave file is stored */ #if !defined (MEDIA_IntFLASH) && !defined (MEDIA_USB_KEY) #define MEDIA_IntFLASH /* Wave file stored in internal flash */ //#define MEDIA_USB_KEY /* Wave file stored in USB flash */ #endif However, when I debug this program, with breakpoints in both #ifdefs for the IntFlash and MEDIA_USB_KEY sections in main(), the executor only runs to the MEDIA_USB_KEY bit, so for some reason it thinks MEDIA USB KEY is defined instead. Can anyone help me out? Thanks