cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F373: SDADC1+DMA2+TIM3

life758
Associate II
Posted on December 17, 2015 at 20:28

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
life758
Associate II
Posted on December 21, 2015 at 11:05

Nobody can help or give me some hints?

Posted on December 21, 2015 at 17:30

That would appear to be the consensus. Forums are often like empty rooms. I don't work with F3 or HAL.

SDADC_EXT_TRIG_TIM13_CC1 // Probably not TIM13

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
life758
Associate II
Posted on December 22, 2015 at 00:35

Thanks Clive!

I have solved the problem after I have update the thread.

The problem was what you pointed out. I copied the wrong string from HAL library.

I had also change the order of some line, as suggested by HAL library

Regards