cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F373 SDADC Clock

s239955_st
Associate
Posted on November 20, 2013 at 10:57

For a project in which I have to measure temperature as well, I would like to run the SDADC continuously but with a slower clock than 500kHz. Concerning the datasheet 500kHz is the minimum. Is there a explanation for this value, or can I go underneath? What do I have to expect when I will run it with 100kHz?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0