STM32F3 Auto-Wakeup problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-11 9:14 AM
Posted on May 11, 2015 at 18:14
Hi All,
I'm studying STM32F3 Low power modes and I need to go in standby mode periodically and wake-up via RTC after n seconds (Run->standby->Run ...).I set the RTC, the wakeup-Timer-IT, I do something in main loop and after these actions I call the standby mode. The system goes in standby and after n seconds, wakeup itself but code doesn't seems to run correctly (it look to be freeze)I feel that there is a miss any flag to be reset.For a moment I left auto-wakeup and I try to wakeup with wakeup-pin 1. System works perfectly Regards
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0