cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207 with external SRAM and NAND

Thomas_Socomec
Associate II
Posted on June 08, 2012 at 09:13

Hello,

I have a question about STM32F207 :

Is it possible to connect an external SRAM + an external NAND flash on the same microcontroller through the FSMC controller ?

What is the effect in this case in term of performances ?

Thank you in advance for your response.

Thomas

#stm32-207-fsmc-nand-sram
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 08, 2012 at 16:28

Sure, they would each need their own chip select line and settings. The bus would adjust to the speed as it accesses the memory space associated with each device.

Suggest you look at the STM322xG-EVAL, both the software and schematics.

http://www.st.com/internet/evalboard/product/250374.jsp

STM32F2xx_StdPeriph_Lib_V1.0.0\Utilities\STM32_EVAL\STM322xG_EVAL

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..