cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107VB i2s in slaveTX mode bug??

kam
Associate
Posted on November 28, 2009 at 10:36

STM32F107VB i2s in slaveTX mode bug??

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
kam
Associate
Posted on May 17, 2011 at 13:32

I have a problem with the I2S interface synchronization in slaveTX mode, the processor does not respond to signals issued on the line WS, below are pictures of osciloscope, upper line is the signal WS and the bottom line is the signal data(0x008A). Interface I2S and GPIO is set correctly. has anyone an idea why this happens ??

http://imgimageshack.us/img177/2372/zdjcie0jpg

http://imgimageshack.us/img137/5159/zdjcie0091c.jpg

mike2001
Associate II
Posted on May 17, 2011 at 13:32

Hi kam.ciaston. I have the same problem. Whether you have solved it or not, please contact me: mike2001 /_at_/ tlen.pl

gregory23
Associate
Posted on May 17, 2011 at 13:32

Hi,

In fact, it's a known issue of STM32F103, STM32F105, STM32F107 devices with I2S feature used in slave mode.

Because in slave mode, the I2S WS signal level is used only to start the communication.

If the first synchronisation with WS is missed, there won't be any re-synchronisation done by the I2S interface.

So be sure to enable the I2S interface at the right moment to synchronize data and clocks (monitor WS signal when at low or high level, depending on I2S audio format).