STM32F105VC USB_HOST MODE ENUMERATE PROBLEM
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-20 3:21 AM
Posted on January 20, 2015 at 12:21
HI,
I try to create a txt file in to a 8gb flash disk (Toshiba 16GB Hayabusa). I have my own board , dm and dp are direct connected vbus sense pin(pa9) is direct connected to 5V power, there is no any usb connection. I used stm3210c-eval firemware and I define it as FS HOST MODE. The problem is when STM32
can not enumerate device and program go to HOST_CTRL_XFER.. So always program go toHOST_CTRL_XFER after this moment..
what stm32 need to enumerate usb flash disk ?Can anyone help me about this....
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0