cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103x8 interupt not working after relocate

ho
Associate II
Posted on November 16, 2016 at 02:56

I have problem after relocating, my interrupt stop working.

A brief explanation about my firmware i) the bootloader (0x08000000) ii) the main application (0x08004000) In my bootloader, I relocate the code as shown below:

pFunction jump_to_application; 
uint32_t jump_address;
#define APPLICATION_ADDRESS 0x08004000
if (((*(__IO uint32_t*)APPLICATION_ADDRESS) & 0x2FFE0000) == 0x20000000) {
jump_address = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);
jump_to_application = (pFunction) jump_address;
_set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);
jump_to_application();
}

and in my main app, I offset the vector table as

NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000);

When i try debug for my bootloader, it is able to relocate to the main app, and the interrupt is working. But, when I power off and power it on, the bootloader can relocate to the main app, but the interrupt in the main app is not working. May I know how can I solve this problem?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ho
Associate II
Posted on November 16, 2016 at 04:00

I managed to fix the problem, but I still dont understand why

SysTick_Config(SystemCoreClock / 1000);

I have enable the SysTick as shown above, but before I jump to my app, I dint not disable this. Now, I changed my code to disable it first before jump, and it works.

SysTick->LOAD = 0;
SysTick->VAL = 0;
SysTick->CTRL = 0;

I have no idea, why this problem happens, and I have similar board using STM32F4 and STM32F2 series, and I jump without disable this and it still works fine. Anyone can enlight me on this?