cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103CB

keng1230
Associate II
Posted on September 12, 2011 at 11:51

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 12, 2011 at 16:39

There have to be a dozen examples posted to the STM32 forums here. Posting yet another example is not going to help you if you have a hardware issue, pin assignment problems, or simply not setting things up properly.

Suggest you post the code you are attempting to use. Provide details of your tool chain, and test board.

Look at the extensive samples provided by Keil and IAR installs, as part of the ST Firmware Library, and review the STM32 manuals. Using three USARTs on the STM32 is quite possible.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..