cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8_USB_Composite_MSC+HID

sonhai26988
Associate II
Posted on December 06, 2014 at 10:35

Dear All.

I'm now working with Composite Example of ST USB Example Project.

Now I can work with both MSC+HID like example, and more modify (change MSC from SD card to Internal Flash). That's ok.

But, I need help from Community, I don't understand why I can't  remove EXTI15_10_IRQn interrupt.

In ST_USB example this interrupt (EXTI15_10_IRQn ) be config to manage the TAMPER button push event. EXTI9_5_IRQn be config to manage user button.

I can easily remove User button.

But when I disable config of EXTI15_10_IRQn, like that:

- in Function void EXTI_Configuration(void):

//  EXTI_InitStructure.EXTI_Line = TAMPER_BUTTON_EXTI_LINE;

//  EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

//  EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling;

//  EXTI_InitStructure.EXTI_LineCmd = ENABLE;

//  EXTI_Init(&EXTI_InitStructure);

//  

//  /* Clear the Tamper EXTI line pending bit */

//  EXTI_ClearITPendingBit(TAMPER_BUTTON_EXTI_LINE);

- in Function void USB_Interrupts_Config(void):

//  NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn;

//  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

//  NVIC_Init(&NVIC_InitStructure);

And the Problem is:

I can't Flash MCU again. And get the alarm ''Failed to read CPUID for Cortex device''...

I must to use Flash Loader Demostator to erase all Internal Flash to can Flash MCU with ST Link again.

How I can remove this interrupt?

Thanks and Best regards.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0