cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0xx_StdPeriphDriver Comparator Speed Setting

oliver
Associate
Posted on July 02, 2013 at 08:21

Hi,

there is a bug in stm32f0xx_comp.h (V1.0.0RC1 / 27-January-2012), which I recently downloaded from the ST website. The comparator speed settings begin with low speed modes, but according to the reference manual (14.4.1 COMP control and status register / p. 227), the high speed ones come first (I can confirm, this is correct).

The code is:

#define COMP_Mode_UltraLowPower                  0x00000000           /*!< Ultra-low power mode */

#define COMP_Mode_LowPower                       COMP_CSR_COMP1MODE_0 /*!< Low power mode */

#define COMP_Mode_MediumSpeed                    COMP_CSR_COMP1MODE_1 /*!< Medium Speed */

#define COMP_Mode_HighSpeed                      COMP_CSR_COMP1MODE   /*!< High Speed */

But should be:

#define COMP_Mode_HighSpeed                  0x00000000           /*!< High Speed */

#define COMP_Mode_MediumSpeed                COMP_CSR_COMP1MODE_0 /*!< Medium Speed */

#define COMP_Mode_LowPower                   COMP_CSR_COMP1MODE_1 /*!< Low power mode */

#define COMP_Mode_UltraLowPower              COMP_CSR_COMP1MODE   /*!< Ultra-low power mode */

You might want to correct it in future versions.

Kind regards

Oliver
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0