cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 HAL UART DMA RX works only once

krzysztof23
Associate II
Posted on May 17, 2015 at 09:44

Hi.

I am trying to write a simple program for DMA rx transfers from UART interface. I am using the HAL drivers and HAL_DMA_Recieve.

The problem I have found is very strange. DMA RX transfer from UART works only once. Then  I have constant UART OR (overrun) bit set and controller does not recieve anything. The strangest thing is that there is no difference between DMA Normal mode and DMA Circular mode for DMA RX.

I have no idea where I should look for the problem.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
krzysztof2399
Associate II
Posted on June 23, 2015 at 20:21

Hi,

I've spent few hours on it, but finally I have solution.

I've found mistake in ''stm32f0xx_hal_uart.c'' file.

There is no condition for Circular Mode in callback function ''UART_DMAReceiveCplt'' line 1572.

Working function should look like:

/**

  * @brief DMA UART receive process complete callback

  * @param hdma: DMA handle

  * @retval None

  */

static void UART_DMAReceiveCplt(DMA_HandleTypeDef *hdma)  

{

  UART_HandleTypeDef* huart = ( UART_HandleTypeDef* )((DMA_HandleTypeDef* )hdma)->Parent;

  if((hdma->Instance->CCR & DMA_CCR_CIRC) == 0)

  {

      huart->RxXferCount = 0;

      /* Disable the DMA transfer for the receiver request by setting the DMAR bit

         in the UART CR3 register */

      huart->Instance->CR3 &= (uint32_t)~((uint32_t)USART_CR3_DMAR);

      /* Check if a transmit Process is ongoing or not */

      if(huart->State == HAL_UART_STATE_BUSY_TX_RX)

      {

        huart->State = HAL_UART_STATE_BUSY_TX;

      }

      else

      {

        huart->State = HAL_UART_STATE_READY;

      }

 

}

  HAL_UART_RxCpltCallback(huart);

}

I hope they'll fix it in next library version.