STM32F and BLE
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-02-26 4:17 PM
Posted on February 27, 2014 at 01:17
I have an existing application that uses a STM32F series MCU and I wish to extend it with Low Energy BlueTooth. I only require BLE not Dual Mode.
I have been looking at the STBLC01. Documentation states that a protocol stack running in the host is released separately in the form of static library for the STM32L.I have several questions:1. Is this static library compatible with STM32F series MCUs?2. a) If not, should I be looking to the BlueNRG?2. b) The BlueNRG documentation states that an SPI based ACI exists. Is a library provided that encapsulates BLE Profiles and connectivity or are we required to write a proprietary version of this portion of the stack?I have a few more questions, but this will help determine direction. Your help is greatly appreciated.Thanks,Darren Moffat
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0