cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube: STM32F334 HRTIM configuration for external pins

tgadeyne
Associate
Posted on August 12, 2016 at 10:48

Hi,

I was trying to configure HRTIM of STM32F334C8T of my STM32F3348DISCOVERY board with STM32Cube and encountered an issue.

I set External Event 6 as:

- Source : External Pin (source 1)

- Polarity : high

- Sensitivity : rising edge

and I want to apply an external event filtering on this event of type Blanking with Latch enabled.

The issue is that I cannot set latch enabled with an external pin source for external event but only latch disabled.

I don't understand why this option is disabled, nothing in Reference Manual mentions that latch is not useable in this case and even ST example HRTIM_TM_PFC use this feature with external pin for external event.

Is there a reason that the feature cannot be selected in this case in STM32Cube ?

Thanks
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on August 12, 2016 at 13:42

Hi gadeyne.thibault,

I have made a tet on the STM32CubeMx, and succseed to configure the filter og the external event source 6. I have attached the .ioc file for you .

-Hannibal-

________________

Attachments :

Test_F334_HRTIM_external_filter.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtpA&d=%2Fa%2F0X0000000aXJ%2F4BE22NdTPVhYmb7ZpW08LQIOAlEGsVlq.7uRfBKq0Z4&asPdf=false