cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube F4 V1.5.0 -- suggested code improvement

mduffy
Associate II
Posted on April 23, 2015 at 03:20

The function (as defined in usbd_cdc.c)

uint8_t  

USBD_CDC_TransmitPacket(USBD_HandleTypeDef *pdev)

in fact returns values of type USBD_StatusTypeDef,

not

 

uint8_t

.

This causes type collisions, and IAR warnings of the form ''enumerated type mixed with another type'' if one does something like this:

USBD_HandleTypeDef handle;

USBD_StatusTypeDef result;

...

result = USBD_CDC_TransmitPacket(&handle)

It would be nice if the types returned by a function match the return type of the function. :)

Affected files are

...\STM32Cube_FW_F4_V1.5.0\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Src\usbd_cdc.c (definition)

...\STM32Cube_FW_F4_V1.5.0\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc\usbd_cdc.h (declaration)

This may occur elsewhere in the HAL, but this is one I have encountered.  I did not perform an exhaustive check.  I presume a lint-like checker would locate similar problems if they exist.

This problem exists in 1.4.0 as well.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0