cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210C-EVAL MEMS IO Expander Initialization / Configuration Failure / Error

intelect
Associate
Posted on March 02, 2011 at 19:26

STM3210C-EVAL MEMS IO Expander Initialization / Configuration Failure / Error

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 17, 2011 at 14:26

With I2C devices that get in weird states, and don't have a RESET pin, you sometimes must clock them out of the failing condition before you can start to talk to them.

You might also want to look at the signalling that is getting the device into a weird state in the first place.

Devices which can switch between SPI and I2C mode can also be problematic if they get into the wrong mode.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..