cancel
Showing results for 
Search instead for 
Did you mean: 

STM32104RBT6 baud rate problem

pranamesh
Associate II
Posted on May 25, 2008 at 14:23

STM32104RBT6 baud rate problem

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
pranamesh
Associate II
Posted on May 17, 2011 at 12:35

[I am new to this, so please help without ambiguity]

I am using the Olimex board STM32-103STK with an STM32104RBT6 mcu. the problem is that for a simple application of UART1 (code attached), I am unable to set the baud rate correctly. For example, if I set the baud to 10400 bps, then the actual baud on the wire is 6944 baud (checked using an LA), which is very strange. I modified an existing USART example (and the olimex bliking LED example). All other files are same as the library from ST site.

The line ''myDelay(8000);'' in my code, is another problem as without this, my bytes on the wire ''keeps changing slightly'', however this is not the primary problem.

I am using CodeSourcery GCC (4.2.3) with Eclipse to build my firmware.

What is wrong :o with my code?

[ This message was edited by: pranamesh on 23-05-2008 21:57 ]

viktor3
Associate II
Posted on May 17, 2011 at 12:35

HSI clock source is not accurate for baudrate generation. Use an external crystal instead.

ivanov-i
Associate II
Posted on May 17, 2011 at 12:35

Pranamesh, the number, which you put in the baudrate register is in fact the divider of the clock frequency:

72000000 / 10400 = 6923 - close to the number, which you measured.

If you need a baudrate of 10400 put 6923 in the register.