cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 in Arduino Format

tim3
Associate II
Posted on November 19, 2008 at 11:24

STM32 in Arduino Format

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tim3
Associate II
Posted on May 17, 2011 at 12:52

Hello

We have cooked up an STM32 board in Arduino format. After hours of wrestling with possible names, we ended up mashing Cortex and Arduino to make Cortino. At least we didn't call it the Artex ;)

Details here:

http://www.bugblat.com/products/cor.html

As you would expect, the Cortino can be flashed via the USB port. One neat feature is access to the serial JTAG debugger from the USB port, so you should be able to debug the thing with no additional hardware once we have gotten the SWJ-DP stub finished. Just in case, we also have a full 20-way JTAG port on board...

Getting an open source GDB stub and/or OpenOCD stub would be a real win for the community. So I would love to here from any expert out there on SWJ-DP who would like to have his name carved in open-source immortality.

Tim

st3
Associate II
Posted on May 17, 2011 at 12:52

Quote:

At least we didn't call it the Artex ;)

Or the Cortina :-W :D