STM32 HAL I2C Problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-11-29 1:56 AM
Posted on November 29, 2016 at 10:56
Hello everyone,
for my current project I am trying to communicate with my STM32F407 Discovery board via I2C. I want to poll different data from it using an Arduino board, similar to a sensor I have. The sensor polling already works and is as follows: I send send the address with a write bit, then a register I want the value from, then I send the slave address once more, only this time with a read bit. I then expect a float.So far I have managed to detect my STM using a scanner I implemented. I have trouble moving on from there though mainly because I do not understand the driver description of the HAL library I suppose.My code://I2C InitializationI2C_HandleTypeDef hi2c1;void InitializeI2C1()
{ __I2C1_CLK_ENABLE(); hi2c1.Instance = I2C1; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.ClockSpeed = 100000; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED; hi2c1.Init.OwnAddress1 = 0x25<<1; if (HAL_I2C_Init(&hi2c1) != HAL_OK) { Error_Handler(); } HAL_NVIC_SetPriority(I2C1_EV_IRQn,0,1); HAL_NVIC_EnableIRQ(I2C1_EV_IRQn); __GPIOB_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStructure.Mode = GPIO_MODE_AF_OD; // GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Alternate = GPIO_AF4_I2C1; HAL_GPIO_Init(GPIOB, &GPIO_InitStructure); HAL_I2C_EnableListen_IT(&hi2c1);}extern ''C'' void I2C1_EV_IRQHandler(){ HAL_I2C_EV_IRQHandler(&hi2c1);}// My code for the (already functioning) detect:void HAL_I2C_AddrCallback(I2C_HandleTypeDef * hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode){}void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef * hi2c){ HAL_I2C_EnableListen_IT(&hi2c1);}void main(){ InitializeI2C1(); while(1) { }}For the next step I am just sending the 1 byte register address. So, on the STM board the question is: what do I do? I assume I still have to have the HAL_I2C_EnableListen_IT, otherwise no transmission will take place, correct? Where in the code should I implement the HAL_I2C_Slave_Receive_IT because if I do it in the HAL_I2C_AddrCallback, the I2C line gets help up and nothing works anymore. The same applies if I put it in my main...Thank you for your time.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-11-30 5:47 AM
Posted on November 30, 2016 at 14:47
Hi BesenSelqnin,
I recommend you to have a look to the ready-to-use example inside the STM32CubeF4 ''I2C_TwoBoards_ComIT'' at this path STM32Cube_FW_F4_V1.14.0\Projects\STM32F4-Discovery\Examples\I2C\I2C_TwoBoards_ComITSee how the I2C state machine is implimented to send and receive data in interruption mode.-Hannibal-