cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 FSMC 512x16bit SRAM address mapping

andrewg
Associate III

hi, i've some questions regarding the use of 16 bit SRAM with FSMC

using AN2784 section 3.3 on SRAM

https://www.st.com/content/ccc/resource/technical/document/application_note/27/bf/f5/e8/d7/82/44/6f/CD00200423.pdf/files/CD00200423.pdf/jcr:content/translations/en.CD00200423.pdf

in the schematic, IS61WV51216BLL SRAM is used which is a 512 x 16 bit word SRAM.

my question is, do the address lines A0-A18 address individual 16 bit words or do that actually address memory in bytes.

e.g. if A0 = 0, A1 = 1, does this address the 3rd 16 bit word or does that address the 3rd byte in the memory instead? the reason for asking is that for one thing this uses the LB (lower byte) and (upper byte) signals to address individual byte, in particular when writing.

the other reason for asking is:

both

IS61WV51216BLL

http://www.issi.com/WW/pdf/61-64WV51216.pdf

and

IS62WV51216ALL/BLL

http://www.issi.com/WW/pdf/62-65WV51216EALL-BLL.pdf

are 512 x 16 SRAM IS62 being the slower one

however, on closely examining the 2 SRAM sku above, i noted that both are 44 pins TSOP

the data lines and all the other control signals are at the same pinouts

however, the address pins order are completely different some of them reversed in order

if the address lines select 16bit words in the SRAM and STM32 does the mapping internally it would be possible to simply swap and exchange the 2 sku. However, if the address lines select bytes instead swapping the chips would cause data to be trashed

would i be able to swap the above 2 SRAM chips for each other in the same pinouts? i.e. are they 'pin compatible'?

thanks in advance !

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

In 16-bit access mode the A0-A18 on the external device represent A1-A19 internally as the STM32 shifts them to be word addresses. The bytes are then selected off the D0-D15 appropriately, with Byte Lane selections when writing.

Your example is for the 3rd word

A1 A0

0 0 Word#0

0 1 Word#1

1 0 Word#2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andrewg
Associate III

oops and Thanks !

Hence in this case when the address is presented to the SRAM e.g. A0 to A18, the SRAM would select distinct (16 bit) words rather then bytes?

That's good as it means the 2 SRAM chips can be swapped for each other despite the different ordering of the address lines

>>Hence in this case when the address is presented to the SRAM e.g. A0 to A18, the SRAM would select distinct (16 bit) words rather then bytes?

Yes

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..