cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 - Burst read external NOR flash

rs11
Associate II
Posted on February 23, 2009 at 12:13

STM32 - Burst read external NOR flash

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
rs11
Associate II
Posted on May 17, 2011 at 13:04

STM32 (Access line, 512KB internal Flash, 48K Internal RAM)

My system's external flash memory reads have a timing constraint, and hence would like to use burst reads from a synchronous flash. Are there any app note or example source code of the processor configuration for burst reading an external flash in synchronous mode? How to set the number of half-words for the burst read. Thanks for any information.