cancel
Showing results for 
Search instead for 
Did you mean: 

ST-One: STM32F4xx ADC Channels

raptorhal2
Lead
Posted on October 18, 2011 at 03:34

The data sheet for the STM32F4 series states that 24 external ADC input channels are available, but I can find only 23 in the pin assignments. ADC3_IN8 appears to be missing.

The F4 reference manual (RM0090) describes just 16 external channels.

Please reply with the pin assignment for ADC3_IN8 and, of course, poke your ST brethren to fix the documentation.

Cheers, Hal

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 18, 2011 at 16:32

Hi Hal,

There are 24 ADC input channel for STM32F4: ADC3_IN8 is mapped on PF10 pin.

Datasheet and RM will be updated.

Cheers,

STOne-32.