cancel
Showing results for 
Search instead for 
Did you mean: 

SPI3 are these values correct?

kemal
Associate II
Posted on January 02, 2018 at 11:40

//stm32f4xx.h

//CS4271 audio CODEC

//GPIOC _I2S_SDO GPIO_Pin_12

//GPIOC _I2S_SDI GPIO_Pin_11

//GPIOC _I2S_SCK GPIO_Pin_10

//GPIOA _I2S_WS GPIO_Pin_15

#define AUDIO_I2S                                             SPI3

#define AUDIO_I2S_EXT                                    I2S3ext

#define AUDIO_I2S_CLK                                    RCC_APB1Periph_SPI3

#define AUDIO_I2S_ADDRESS                          (SPI3_BASE + 0x3C00)    //Are these values correct?

#define AUDIO_I2S_EXT_ADDRESS                 (I2S3ext_BASE + 0x4000) //Are these values correct?

#define AUDIO_I2S_GPIO_AF                            GPIO_AF_SPI3

#define AUDIO_I2S_IRQ                                     SPI3_IRQn

#define AUDIO_I2S_EXT_                                   IRQ SPI3_IRQn

#define AUDIO_I2S_IRQHandler                         SPI3_IRQHandler

#define AUDIO_I2S_EXT_IRQHandler                SPI3_IRQHandler

#define AUDIO_I2S_DMA_CLOCK                      RCC_AHB1Periph_DMA1

#define AUDIO_I2S_DMA_STREAM                    DMA1_Stream5

#define AUDIO_I2S_DMA_DREG                         AUDIO_I2S_ADDRESS

#define AUDIO_I2S_DMA_CHANNEL                  DMA_Channel_0

#define AUDIO_I2S_DMA_IRQ                             DMA1_Stream5_IRQn

#define AUDIO_I2S_DMA_FLAG_TC                   DMA_FLAG_TCIF5

#define AUDIO_I2S_DMA_FLAG_HT                   DMA_FLAG_HTIF5

#define AUDIO_I2S_DMA_FLAG_FE                   DMA_FLAG_FEIF5

#define AUDIO_I2S_DMA_FLAG_TE                   DMA_FLAG_TEIF5

#define AUDIO_I2S_DMA_FLAG_DME                DMA_FLAG_DMEIF5

#define AUDIO_I2S_EXT_DMA_STREAM            DMA1_Stream2

#define AUDIO_I2S_EXT_DMA_DREG                 AUDIO_I2S_EXT_ADDRESS

#define AUDIO_I2S_EXT_DMA_CHANNEL          DMA_Channel_2

#define AUDIO_I2S_EXT_DMA_IRQ                     DMA1_Stream2_IRQn

#define AUDIO_I2S_EXT_DMA_FLAG_TC           DMA_FLAG_TCIF2

#define AUDIO_I2S_EXT_DMA_FLAG_HT           DMA_FLAG_HTIF2

#define AUDIO_I2S_EXT_DMA_FLAG_FE           DMA_FLAG_FEIF2

#define AUDIO_I2S_EXT_DMA_FLAG_TE           DMA_FLAG_TEIF2

#define AUDIO_I2S_EXT_DMA_FLAG_DME        DMA_FLAG_DMEIF2

#define I2S_STANDARD                                        I2S_Standard_Phillips

    stm32f4xx.h is writing.

(SPI3_BASE   +   0x3C00)

(I2S3ext_BASE + 0x4000)

I'm not sure right?

                             Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on January 02, 2018 at 18:18

Probably no, but that depends on usage of those symbols.

JW