2013-07-18 12:57 AM
I am using the STM32L151RBH6 which I believe is a medium density device, I am trying to get SPI working using the STM32Lxx_spi.c library but from reading the header at the top of V1.1.1 the I2S feature is not working for my device.
My questions are:1) Is the V1.1.1 the latest peripheral library?2) If I cannot use the SPI_I2S_SendData() command is my only option using DMA or writing my own driver? Does anyone know if DMA SPI works on medium density devicesThanksTom2013-07-18 4:28 AM
1) No.
http://www.st.com/web/en/catalog/tools/PF257913