cancel
Showing results for 
Search instead for 
Did you mean: 

SPI input value being interpreted incorrectly

bnp979
Associate III
Posted on January 05, 2015 at 08:33

My project involves using a STM32L152 device as a SPI master that receives data from a slave (digital accelerometer). When I look at the SPI signals through a scope, I notice that the incoming SPI data is being interpreted incorrectly by the L1 device.

I use the STM32CubeMX GUI to generate the code for the project. I am wondering if

whether my usage of the tool is somehow causing this issue or

 if there are known issues relating to the tool causing these issues. 

I have attached images showing the oscilloscope outputs for an example case where I am finding the error. The blue signal represents SPI clock and yellow is SPI Data In.

The case involves two bytes being read from the SPI port (corresponding to 2 sets of 8 clock cycles in the SPI clock). The second byte clearly has ''data in'' line being zero throughout. Yet the data is being read as a 1.

I am consistently seeing these sort of errors where the LSB is being wrongly interpreted as a '1' sometimes when it should be a 0 and vice versa.

Here are the SPI initialization settings generated by Cube.

  hspi1.Instance = SPI1;

  hspi1.Init.Mode = SPI_MODE_MASTER;

  hspi1.Init.Direction = SPI_DIRECTION_2LINES;

  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;

  hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

  hspi1.Init.NSS = SPI_NSS_SOFT;

  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;

  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi1.Init.TIMode = SPI_TIMODE_DISABLED;

  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

  HAL_SPI_Init(&hspi1);

Here is the call I make to read the SPI port:

HAL_SPI_TransmitReceive(&

hspi1, (uint8_t *)&data, (uint8_t *)&temp, 1, 5000);

I'd appreciate any inputs on helping me track the issue. Note that I am driving the CS logic using my own software logic using GPIO and not the hardware based NSS signal.

I'd appreciate any inputs on helping me track the issue.

Thanks,

Ben

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0