SPI Full duplex application
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-02-25 6:16 AM
Posted on February 25, 2012 at 15:16
Hi good people,
I use my MCU as an SPI slave module. application description: It is connected to an SPI generator which sends 8 different words(each word is 16 clks) repeatedly. (1Mhz) : 0x0001, 0x0002,..., 0x0008,0x001,0x0002,... every time i receive 0x0002 , i need to send on the next cycle 0x0800 every time i receive 0x0003 , i need to send on the next cycle 0x0400 My system clock is 24MHZ so i want the application to be as fast as it can. Can you give me a hint how can i implement it (use IRQs , polling ? ) some example code can really help me.. thanx! :)
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0