cancel
Showing results for 
Search instead for 
Did you mean: 

SNMP client (not agent) examples?

bhakan
Associate II
Posted on October 04, 2016 at 19:25

Hello

I've searched almost everywhere but I can't find any example of an SNMP client code. What I'm trying to do is to issue simple SNMP Get/GetNext/Walk commands from an STM32F429 (lwIP) in order to query values from an SNMP agent.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on October 12, 2016 at 13:41

Hi sezgin.hakan,

There is no SNMP example currently available in the Cube package.

I raise your request internally to check if it is possible to add such example. Thanks for sharing.

Then we wait for other Community members, may be they can help with their own solutions.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.