cancel
Showing results for 
Search instead for 
Did you mean: 

Single GPIO initialization for both F1 and F3/F4 series

eliast1234
Associate II
Posted on May 04, 2015 at 20:43

Hi,

I'm trying to write a custom initialization for GPIO of F1 and F3/F4 series. I've defined most of the MODE and IO types but stuct at alternate input mode. F1 series puts the pin to input mode while F3/F4 just sets AF mode. So I've come up with the following pseudocode.

   

// alternate function input

   

&sharpif defined(__F3) || defined(__F4)

   

// F3 series (later F4 as well)

    AF_INPUT_PN     => .GPIO_Mode = GPIO_Mode_AF, .GPIO_PuPd = GPIO_PuPd_NOPULL

//omit .GPIO_OType

    AF_INPUT_PU     => .GPIO_Mode = GPIO_Mode_AF, .GPIO_PuPd = GPIO_PuPd_UP

//omit .GPIO_OType

    AF_INPUT_PD     => .GPIO_Mode = GPIO_Mode_AF, .GPIO_PuPd = GPIO_PuPd_DOWN

//

omit

.GPIO_OType

    + GPIO_PinAFConfig(...)

   

&sharpelse

// __F1 series

   

// F1 series

    AF_INPUT_PN     => .GPIO_Mode = GPIO_Mode_IN_FLOATING

    AF_INPUT_PU     => .GPIO_Mode = GPIO_Mode_IPU

    AF_INPUT_PD     => .GPIO_Mode = GPIO_Mode_IPD

    + GPIO_PinRemapConfig(...)

   

&sharpendif

Do you think it is correct?

#gpio-alternate-input
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0