cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM help

Chuev.Vladimir
Associate III

Hello.

I want to use AS4C8M32SA-6BIN ( https://www.alliancememory.com/wp-content/uploads/pdf/dram/Alliance%20Memory_256M%20SDRAM_AS4C8M32SA-6_7BIN(BCN)%20A%20die_rev%201.0%20November%202016.pdf )

But I can't pick up the settings.

The names in HAL and the name in datasheet are different.

I ask for help to properly adjust my SDRAM

	/* hsdram1.Init */
	hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
	hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
	hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
	hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
	hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
	hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_1;
	hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
	hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_DISABLE;
	hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE;
	hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
	
	/* SdramTiming */
	SdramTiming.LoadToActiveDelay = 16;
	SdramTiming.ExitSelfRefreshDelay = 16;
	SdramTiming.SelfRefreshTime = 16;
	SdramTiming.RowCycleDelay = 16;
	SdramTiming.WriteRecoveryTime = 16;
	SdramTiming.RPDelay = 16;
	SdramTiming.RCDDelay = 16;

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

What STM32 platform? Running at what speed? Details and specifics are important.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Chuev.Vladimir
Associate III

Oh, sorry.

I use STM32H743XIH6

I have 160MHz FMC