cancel
Showing results for 
Search instead for 
Did you mean: 

SDK support for STEVAL-IDS001Vx boards?

eric
Associate
Posted on July 31, 2013 at 21:27

I just started on a hardware dev project and want to use the STEVAL-IDS001V5 board in an embedded ARM9 with Linux. I downloaded the SDK linked from the board's product page but nothing in the SDK appears to support this USD board (instead it supports the ST32 eval motherboard dev kit).

Am I missing something & it does support it? If so, can someone point me to a code example?

If not, is the product just too new and the SDK hasn't been updated yet?

My general plan was to see how it works in Windows, use a USB sniffer to determine the proper data packets, then write support in Linux via libusb so I can put it into the embedded device.

#source-code #steval-ids001vx
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0