cancel
Showing results for 
Search instead for 
Did you mean: 

SD card writing in DMA mode.

rajesh23
Associate II
Posted on September 19, 2016 at 09:55

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
rajesh23
Associate II
Posted on September 22, 2016 at 14:04

Hi

is any one there ?

i asking a simple Question how use a DMA for SD card Read and write ?.

Regards

Rajesh

rajesh23
Associate II
Posted on September 22, 2016 at 14:05

Hi

is any one there ?

i asking a simple Question how use a DMA for SD card Read and write ?.

Regards

Rajesh

Posted on September 22, 2016 at 15:42

is any one there ? i asking a simple Question how use a DMA for SD card Read and write ?

This is a user forum, it appears evident there isn't anyone here right now who can answer your specific question in the context it is being framed, that's how forums work, sometime they can be like an empty room, other times it is full of people who can't answer their own basic questions, and aren't interested in others issues.

There are other avenues to seek help, the Online Support process, talking with your local ST staff or FAE, or engaging a contractor/consultant.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Walid FTITI_O
Senior II
Posted on September 22, 2016 at 16:24

Hi d.rajesh.001,

I am analyzing your request.

Your description of the issue is general . Try to apply the following:

* You should Add a check after read/write operation using HAL_SD_CheckWriteOperation() to check the completion of the write or read process by SD. (You can refer to SD example in STM32cube and follow implementation there)

* If the issue still exist try to debug and localize where the code hangs/stop and the kind of message gives.

You did not precise the version of the drivers / STM32cube you are using . Is-It the last version ?

-Hannibal-
rajesh23
Associate II
Posted on September 22, 2016 at 18:18

Sir,

You did not precise the version of the drivers / STM32cube you are using . Is-It the last version ?

I am using the code demonstration code which has came with the product and i'am not using the STM32 cubemx.

In main header i have found the details below

 * @file    main.c

 * @author  MCD Application Team

 * @version V1.0.1

 * @date    25-June-2015

 * @brief   This file provides main program functions

          here i have given the below code i have tried in tat you can see the ''

uint8_t buffer[512];

''

    

that declared inside the main which leads to read null data at SD read output at DMA mode.

The problem solves if it declared above main i.e Global to main function why this happens ?.

01.

int

main( 

void

)

02.

{

03.

    

/* Configure the MPU attributes as Write Through */

04.

    MPU_Config();

05.

    

/* Enable the CPU Cache */

06.

    CPU_CACHE_Enable();

07.

    

/* STM32F7xx HAL library initialization:

08.

     

- Configure the Flash ART accelerator on ITCM interface

09.

     

- Configure the Systick to generate an interrupt each 1 msec

10.

     

- Set NVIC Group Priority to 4

11.

     

- Global MSP (MCU Support Package) initialization

12.

     

*/

13.

    HAL_Init();

14.

    SystemClock_Config();

15.

    BSP_LED_Init(LED1);

16.

    BSP_LED_Off(LED1);

17.

    uartInit();

18.

    SDdetectInit();

19.

    BSP_SD_Init();

20.

21.

  uint8_t buffer[512];

22.

  uint32_t  count =63;

23.

24.

  HAL_Delay(500);

25.

26.

27.

  

if

( BSP_SD_ReadBlocks_DMA((uint32_t*)buffer,(uint64_t) (512L*count), (uint32_t) 512, (uint32_t) 1) != MSD_OK)

28.

  {

29.

      HAL_UART_Transmit(&UartHandle,

''Read failed''

,

sizeof

(

''Read failed''

),500);

30.

  }

31.

  

else

32.

  {

33.

      HAL_UART_Transmit(&UartHandle,buffer,512,500);

34.

  }

similarly i have problem when i have interfaced with FAT FS it was not working It gives DMA readout timer expires.

01.

void

fatfile_read(

void

)

02.

{

03.

04.

  FRESULT res;                                          

/* FatFs function common result code */

05.

  uint32_t byteswritten, bytesread;                     

/* File write/read counts */

06.

    

if

(FATFS_LinkDriver(&SD_Driver, SDPath) == 0)

07.

    {

08.

      

if

(f_mount(&SDFatFs, (TCHAR 

const

*)SDPath, 0) != FR_OK)

09.

      {

10.

        Error_Handler();

11.

      }

12.

      

else

13.

      {

14.

          

if

(f_open(&MyFile, 

''STM32.TXT''

, FA_READ) != FR_OK)

15.

          {

16.

            Error_Handler();

17.

          }

18.

          

else

19.

          {

20.

              res = f_read(&MyFile, rtext, 

sizeof

(rtext), (UINT*)&bytesread);

21.

              getStringFromWord(rtext,bytesread);

22.

              

if

((bytesread == 0) || (res != FR_OK))

23.

              {

24.

25.

              }

26.

              

else

27.

              {

28.

29.

              }

30.

          }

31.

          f_close(&MyFile);

32.

      }

33.

    }

34.

//    FATFS_UnLinkDriver(SDPath);

35.

36.

}

And fatfs was not working with DMA.

Thanks and regards

Rajesh

Walid FTITI_O
Senior II
Posted on September 22, 2016 at 18:54

Hi d.rajesh.001,

It is normal; you are not respecting here the C coding specification. You want to put data on a local buffer with a scope on stuck through DMA which is not affordable. You should user a global variable with a scope on heap to allow DMA successfully transfer the data from SD to memory buffer.

-Hannibal-