cancel
Showing results for 
Search instead for 
Did you mean: 

RTC

lucas23
Associate II
Posted on July 21, 2015 at 21:18

Hi,

I am using Cube MX to generate the RTC code.

It is working perfectly fine, the time is counted correctly. But every time I turn off the device, the time and date are set back to 0.

I found the problem in the Init function. Every time the RTC is initialized, the time and date are set to zero again.

I solved the problem just by commenting those lines, but I am wondering why cube generates such code! Once that the code is not supposed to be edited, every time I generate a new version I must remember to go there and comment those lines. It is weird. Am I doing something wrong?

/* RTC init function */

void MX_RTC_Init(void)

{

  RTC_TimeTypeDef sTime;

  RTC_DateTypeDef sDate;

  RTC_AlarmTypeDef sAlarm;

    /**Initialize RTC and set the Time and Date 

    */

  hrtc.Instance = RTC;

  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;

  hrtc.Init.AsynchPrediv = 127;

  hrtc.Init.SynchPrediv = 255;

  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;

  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;

  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;

  HAL_RTC_Init(&hrtc);

  // Manually commented

  //sTime.Hours = 0;

  //sTime.Minutes = 0;

  //sTime.Seconds = 0;

  //sTime.SubSeconds = 0;

  sTime.TimeFormat = RTC_HOURFORMAT12_AM;

  sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;

  sTime.StoreOperation = RTC_STOREOPERATION_RESET;

  HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BCD);

  // Manually commented

  //sDate.WeekDay = RTC_WEEKDAY_MONDAY;

  //sDate.Month = RTC_MONTH_JANUARY;

  //sDate.Date = 1;

  //sDate.Year = 0;

  HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BCD);

    /**Enable the Alarm A 

    */

  sAlarm.AlarmTime.Hours = 0;

  sAlarm.AlarmTime.Minutes = 0;

  sAlarm.AlarmTime.Seconds = 0;

  sAlarm.AlarmTime.SubSeconds = 0;

  sAlarm.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;

  sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;

  sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;

  sAlarm.AlarmMask = RTC_ALARMMASK_NONE;

  sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;

  sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;

  sAlarm.AlarmDateWeekDay = 1;

  sAlarm.Alarm = RTC_ALARM_A;

  HAL_RTC_SetAlarm(&hrtc, &sAlarm, FORMAT_BCD);

}

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
petr239955
Associate III
Posted on January 06, 2016 at 13:17

Hi STM32Cube-T,

I have same problem.

When

you

fix

this ?

Petr

tekampe
Associate II
Posted on March 17, 2017 at 17:36

Hi ST

I have same problem.

When

you

fix

this ?

Jens

Posted on March 19, 2017 at 12:38

Hi tekampe.jens,

Maybe you are using an old CubeMx version. If it is the case, I recommend you to use the last version available V 4.20.

Then, if the problem is not resolved, it should be better to create a new discussion describing your use case and giving more details about your issue.

You can also share your .ioc file, this will help user forum and ST team to check your case and answer you.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
bet
Associate II
Posted on April 07, 2017 at 14:54

The same question was posted here:

https://community.st.com/0D50X00009Xka36SAB

I provided a workaround if it helps anyone.

Regards,

Bertrand.