cancel
Showing results for 
Search instead for 
Did you mean: 

resistor placement in crystal path in stm32f4discovery

armindavatgaran
Associate III
Posted on May 29, 2015 at 21:23

Hello

According to UM1472(stm32f4discovery manual) there are 0 and 220 ohm resistors placed in crystal path to pin, why?

Thanks.

1 REPLY 1
Posted on May 29, 2015 at 21:42

It allows for a broader selection of crystals to be used in the design. Understand that crystals can be cut in different directions, and have different resistive and capacitive characteristics. You'd need to review a few crystal specs from a couple of manufactures to understand the options. The boards could also use crystal of different frequencies, 8 MHz is one option, but there are magic values that work for TV frequencies, or baud rates, ethernet, etc. Most of the EVAL series boards use 25 MHz HSE for Ethernet use cases, the DISCO/NUCLEO boards typically derive 8 MHz from an oscillator source provided by the ST-LINK chip. The F4-DISCOs are one of the few that have an 8 MHz crystal and parts placed on main processor.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..