2009-04-29 2:12 AM
PWM through TIM1_CH2N
2011-05-17 4:10 AM
Hello guys,
I made a mistake on the last PCB layout and atatched two different things in TIM3. I found out that the buzzer I want to use can be remapped to TIM1_CH2N because it's connected to PB0. Unfortunately I did not get this (special) output to work. Can anyone supply me with an as-simple-as-possible-solution for getting a rectangular wave (2kHz for a buzzer) out of TIM1_CH2N using the STM32FWlib. regards Christoph [ This message was edited by: gommel on 29-04-2009 14:43 ]