cancel
Showing results for 
Search instead for 
Did you mean: 

ptp initialisation on stm32F407

431023
Associate
Posted on March 23, 2015 at 16:58

Hallo,

Regarding STM32F407ZGT6 controller chip on an Olimex stm32-e407 board.

I have a problem with initializing the fine adjustment for the PTP block

The TSARU bit does not return to 0 after setting it.

I wonder if someone might throw some light on this.

Here is the sequence of operations:

-----------------------------------

reset the board,

download the flash image

continuous step to breakpoint just before the problem

and then single step thru the problem zone.

also running the board without the debugger attached gives a hung board

in the ptp init area.

Here is an abbreviated program listing (from start up):

------------------------------------------------------

(the registers are loaded in a temp reg and the bits are set as needed

then temp registers are written back. This is to help reading the prog. and avoid partial writes)

  ( Reset_Registers  -- reset bits: Off, Reset, Off )

-- select media interface for ETH

      PMC_Tmp.MII_RMII_SEL    := Scfg.RMII;

-- write to hardware

      R.Syscfg.PMC            := PMC_Tmp;

-- start some clocks:

      Ahb1en_Tmp.GPIOA     := Rcc.Enable;  -- for eth_rmii interface pins

      Ahb1en_Tmp.GPIOB     := Rcc.Enable;  --

      Ahb1en_Tmp.GPIOC     := Rcc.Enable;  -- for eth_rmii interface pins

      Ahb1en_Tmp.GPIOG     := Rcc.Enable;  -- for eth_rmii interface pins

-- write to hardware

      R.Rcc.AHB1ENR        := Ahb1en_Tmp;

     ( Init_Pins        -- amonst others for the ETH block )

-- start the ptp clock

      Ahb1en_Tmp.ETHMACPTP := Rcc.Enable;

      R.Rcc.AHB1ENR        := Ahb1en_Tmp;

( init usart 6, incl. dma)

      Finrod.Board.Init_Eth_Clock; -- positioned this in various places

                                   -- but it has to be before the PTP control

                                   -- register gets updated (apparently)

-- no interrupts

      Macimr_Tmp.TSTIM       := Eth.Int_Disabled;

      R.Eth_Mac.Macimr       := Macimr_Tmp; -- write it

      

-- enable time stamping

      Ptpt_Control_Tmp.Tse        := Eth.Enabled;

      Ptpt_Control_Tmp.TSSIPV4FE  := Eth.Enabled;

      Ptpt_Control_Tmp.TSSARFE    := Eth.Enabled;

      Ptpt_Control_Tmp.TSPTPPSV2E := Eth.Enabled;

      Ptpt_Control_Tmp.Tsaru := Eth.Off; -- for the unfathomable reason

                                         -- this might work

      R.Eth_Mac.PTPTSCR      := Ptpt_Control_Tmp; -- write it

( small delay loop)

      PTP_SSIR_Tmp.Stssi     := 43;

      R.Eth_Mac.PTPSSIR      := PTP_SSIR_Tmp;  -- write it;

      R.Eth_Mac.PTPTSAR      := 3_652_183_076; -- write it directly, its 32 bits

      

      -- update it, and wait for it to be done

      Ptpt_Control_Tmp.Tsaru := Eth.Update;

      R.Eth_Mac.PTPTSCR      := Ptpt_Control_Tmp; -- write it

      while Ptpt_Control_Tmp.Tsaru /= Eth.Off loop

     Ptpt_Control_Tmp    := R.Eth_Mac.PTPTSCR;

      end loop;

 

And this loop never ends  . . . . . . .

I have attached a pdf with the debugger output of the registers affected, at the time of the endless loop.

I did cross check against the hardware errata and against the CMSIS library.

Regards,

Jan de Kruyf.

#ptp-init-stm32f407
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0