cancel
Showing results for 
Search instead for 
Did you mean: 

Problem Writing in an I2C EEPROM using CPAL

sajjadi335
Associate
Posted on March 16, 2014 at 06:53

Hi

On an STM32F103, I have used CPAL example for basic EEPROM. 

I have a function which writes 16 bytes to the EEPROM, and it is used only twice in a row, to write to different addresses.

Frequently, I encounter one of the following problems:

- A DMA TX Error

- repeated start bit event.

What is the problem in my code?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0