cancel
Showing results for 
Search instead for 
Did you mean: 

Problem adding a Module GUI Demonstration Builder Firmware

eduardo2
Associate II
Posted on August 15, 2014 at 18:22

Hi:

I have followed the documentation UM1550 STM32 Demonstration Builder developer guide, at Chapter 5 Bulding a Module. Also I have used the template file provided with the Demo, to add this new module and I was successful to include an icon in the right location.

Now, when I click in the icon the code goes nowhere at: (highlighted part)

static void TEMPLATE_INFO_SwitchPage(GL_Page_TypeDef* pParent, uint32_t PageIndex)

{

  /* Switch to new page, and free previous one. */

  GL_Page_TypeDef* NextPage = NULL;

  (*pParent).ShowPage(pParent, GL_FALSE);

  DestroyPage(pParent);

 

vPortFree(pParent);

  pParent = NULL;

  if (PageIndex == PAGE_MENU)

  {

    GL_ShowMainMenu();

    return;

  }

vPortFree is a FreeRTOS function is a call to free up RAM, but it may be a pointer problem where there's no definition of the pointer or something, I don;t know.

The original Modules work ok. I am missing something here?

Please help, Thanks.

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0