cancel
Showing results for 
Search instead for 
Did you mean: 

Possible bug in AN3109

diego239955_st
Associate
Posted on March 20, 2010 at 09:52

Possible bug in AN3109

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
damh
Associate II
Posted on May 17, 2011 at 13:44

This code is risky.

I don't see the initialization of the counters and DMA. DMA transfer size/counter should be below or equal 250.

Is RxBuffer2_SW used for more than one DMA packet? If not, why are there 2 counter variables RxCounter1 and RxCounter?

Why do you use copy instead of changing the DMA buffer? Changing DMA buffer is easier and faster ;)
Posted on May 17, 2011 at 13:44

http://www.st.com/stonline/products/support/micro/files/an3109.zip

The problem is that the code in the application note is ILLUSTRATIVE, it is not a general solution which can be dropped into your application. For example it disables DMA once it interrupts instead to reinitializing it for the next burst of data.

I generally agree that the DMA Rx data should be double buffered, and set up as a circular transfer, too address a couple of latency issues.

-Clive

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
marbel
Associate II
Posted on May 17, 2011 at 13:44

Hi,

I have also been looking at the AN3109.  My goal is simply to remove as many interrupts as possible from my system. When I run the system, it generates interrupts periodically and is not at all depending on transfers on my UART TX line. I would have wished for a solution where the rising edge starts and resets the timer. Am I missing something here?

// Martin